Transformer Relays - DP300

The DP-300 is universal in its applications. By selecting the vector group in the display, users can change the phase shift of the transformer without having to worry about changing the connection of the external current transformers (CTs). The different nominal currents of the high and low voltage side of the transformer, as well as the transformer ratio, may be configured and every measuring point may be set separately.