35kV cutout 264x168

40.5kV Cutout

40.5kV fuse Cutout is focusing on the wind farm market.The polymer inssulator is lighter than the pocerlain one,which reduce the wind force put on the cutout body. This Cutout has the full testreport released by Suzhou Hight Voltage Test lab. All the parameters meet the wind farm's requirements . This cutout can protect the transformer from the fault current and work as a Disconnector when the curent shut down.