Model 570 Multi-Basket 8-24 inch

Duplex strainers remove damage causing particulate matter from the process media, and never have to be shut down for cleaning…the line can run continuously. When one set of strainer baskets becomes full in the Model 570 multi-basket strainer, flow is switched to the other set. The first set of basket is removed, cleaned and are ready for use again.