下载文档 () / 20
Support service

Insert molding

We are a leader in insert – also known as over molding – due to our proprietary cavity centering technology (CCT). CCT constrains the busbar to the center of the mold cavity during the injection molding, preventing high scrap rates or marginally passing Hi Pot™ parts to escape the plant. An unsupported busbar is significantly impacted by the injection molding melt front as the plastic fills the cavity.

Depending on several factors, the plastic may fill top or bottomed influenced because the busbar is not stable. One of our many specialties is insert and injection molding and in-mold assembly. We operate in-house, high-speed metal stamping and insert-injection molding. Machining units in this department exert a clamping force ranging from 30 to 310 tons with a varied number of cavities while employing tight tolerances.

核心功能

  • Machining units exert a clamping force ranging from 30 to 310 tons with a varied number of cavities while employing tight tolerances
  • Cavity centering technology lowers scrap rates
  • Robust vibration resistance