下载文档 () / 20
动力,因我们而不同*

Unforgettable artistic experiences in Helsinki Opera House

Discover how Eaton enables successful performances at the Finnish National Opera and Ballet

“We are extremely pleased with the project and the new Eaton UPS devices. We value the fast response time of the maintenance services, too.”

Timo Koskinen, Electrical Engineer, the Finnish National Opera

It is essential to ensure the performances on stage are not interrupted by technical issues

Since 1993, the Finnish National Opera and Ballet has operated at its current premises in the Helsinki Opera House. It attracts an audience of almost 300,000 people every year. The goal of the Finnish National Opera and Ballet is to offer unforgettable artistic experiences for its visitors. Therefore, the stage technology must work flawlessly during performances and rehearsals.

The old system had to be replaced and the new system of the Opera House had to be uniform.

When a performance is taking place, there are a lot of people on stage and inside the hall. The technical personnel are busy making sure the technology works flawlessly in all aspects to ensure a uninterrupted performance. The old UPS system was not well set-up and subsequently, it could take a long time to find the fault. All devices had to be supplied by the same supplier and comprehensive life cycle services and technical support must be available.

A uniform solution which includes comprehensive life cycle services and technical support for the devices.

The new UPS system of the Opera House includes Eaton 93PS UPS devices and Eaton 9SX UPS devices of three efficiency levels as well as an additional set of batteries. The provided UPS devices include an external bypass switch which makes sure that power is not cut off even when the UPS does not work. The system has a comprehensive technical support and maintenance agreement.

Read the full story

Download the full story here

Discover Eaton 91PS & 93PS UPS

Eaton 91PS and 93PS provide the lowest Total Cost of Ownership and maximum availability in its power range. Whatever your mission-critical application, the Eaton 91PS and 93PS UPS offer the power performance, scalability, resiliency and efficiency you need for cost-efficient business continuity.