下载文档 () / 20
动力,因我们而不同*

Location: Detroit, Michigan 

Segment: Recycling

Challenge: Protect an ultra filtration unit used in a wash water recycling system

Solution: A pair of Eaton DCF-1600 mechanically cleaned filters using 0.006” slotted element media.

Results: Extended ultra filter life by eliminating small titanium particles in the wash water stream. The estimated return on investment is less than six months, based on the amount of particulate retained and water savings.

The Eaton filters are part of a large water treatment project that helped reduce our water consumption by 75 percent. The filters are working as expected, and the customer service from Eaton has been outstanding.

Jesse Oliver, Plant Engineer Global Titanium

Background 

Titanium is an essential material in a broad range of aerospace applications due to its light weight and high strength.

Global Titanium of Detroit, Michigan purchases titanium chips and turnings from manufacturers around the world and recycles more than a million pounds of them each month for use by producers of titanium, steel, stainless steel, aluminum and powder metallurgy products.

The chips are crushed and then washed with water on a side hill screen which captures the large pieces, but allows particles smaller than 230 microns to pass through into the waste water stream. The company recycles wash water on site through an ultra-filtration system and then reuses it to comply with environmental regulations. 

Challenges

The small titanium particles were damaging the ultra filter, necessitating the use of a prefilter. Global Titanium needed to recover the titanium particles as an additional source of recyclable material while handling 100,000 gallons of water per day used in the washing process. Global Titanium also required a selfcleaning filter using permanent media to minimize downtime and maintenance.

"The titanium chips contain every kind of contaminant imaginable: coolant, dirt, plastic and cardboard," said Jesse Oliver, plant engineer at Global Titanium. "The primary contaminant is cardboard, which produces long, stringy fibers that are hard to handle." 

Solution 

The customer rented an Eaton DCF-800 mechanically cleaned filter to test the feasibility of prefiltering the waste water stream.

"The startup went well although the solids loading was high, requiring a purge every ten minutes," reported Eaton regional sales manager, Bruce Law. "The customer was encouraged by the filter's performance and the amount of titanium that was retained. Customer Success Story: Global Titanium Market Served Manufacturing & Industrial

They sampled several different element retentions and eventually decided on the .006 inch (150 micron) slotted element because it most efficiently removed titanium particles while maintaining the required system flow and pressure."

DCF series filters are believed to be among the most efficient mechanically cleaned filters currently available. Operating at consistently low differential pressures, they deliver simple, reliable operations with a low initial investment.

The DCF filter consists of a cylindrical stainless steel housing that holds the filter media, in this case a slotted element. Fluid enters inside the element and flows through to the outlet, depositing any contaminants on the inside of the element.

A spring-loaded cleaning disc moves up and down, wiping the filter element clean and depositing the contaminants at the bottom of the housing, out of the flow path. Because the filter remains in service while being cleaned, DCF filters support high process efficiency while minimizing cleaningrelated product loss. 

Results 

Based on the performance of the test system, Global Titanium purchased two DCF self-cleaning filters within 45 days of the completion of the rental. Both units are used to protect the ultra filter from two different water sources in the plant.

When the customer evaluated the best possible location for the new filters, the flow rates indicated that they needed to purchase DCF-1600 models rather than the DCF-800 that was used in the trial. Both of the DCF-1600 filters use .006 inch media to handle the volume of wash water with an extended purge cycle.

"The Eaton filters are part of a large water treatment project that helped reduce our water consumption by 75 percent", said Jesse Oliver. "The filters are working as expected, and the customer service from Eaton has been outstanding."

The estimated return on investment is less than six months, based on the amount of particulate retained and water savings.

Eaton's DCF Self Cleaning Filter

DCF series filters are believed to be among the most efficient mechanically cleaned filters currently available. The Eaton DCFseries of mechanically cleaned filters is ideal for highly viscous, abrasive, or sticky liquids. The DCF mechanically cleaned filters operate at a consistently low differential pressure and deliver simple, reliable operation in which a low initial investment is a key driving factor.