下载文档 () / 20
动力,因我们而不同*

Location: Haag, Austria

Segment: Beverages, spirits

Challenge: Selective distillate filtration

Solution: BECO SELECT A depth filter sheets range and BECO standard range

Results: Filtration solutions to an awardwinning distiller, enabling the production of high-quality, turbidity-free spirits with full flavor


With the BECO SELECT A depth filter sheets and the BECO standard range from Eaton, we have succeeded in exactly what we want to achieve in filtration: Getting the best results from fine distillates

Georg Hiebl, George Hiebl Distrillery

Background

In 1993, Georg Hiebl took over the distillery from the family agricultural business and, together with his brother Robert, gave it a new economic direction – producing quality distillates. In 1997, the company purchased a 150 L rectification distillery plant and built a new mashing room. To ascertain the level of quality of the products at the time, the brothers entered four product samples at the ‘Destillata’ fine-spirit awards. Winning one silver and two bronze medals on their first visit was evidence that the company was already well on its way. More success soon followed. As early as 1999, they won their first gold medal and since then they have been established in the winners’ circle and have taken the overall prize on several occasions. In 2013, they entered 52 samples and received 51 medals, 19 of them gold, winning such awards as “Distillates of the Year” and even gaining record-breaking maximum points in some categories. Their unprecedented success in German-speaking countries was soon followed in international competitions, such as the “International Wine and Spirit Competition (IWSC)” in London, where the Hiebls were named “Boutique Distiller of the Year 2014”. The secret of their success lies in choosing the best raw ingredients, thorough fermentation and distillation processes and the use and specific combination of filtration solutions from Eaton’s Filtration division. 

Challenge 

In terms of the raw ingredients, which come primarily from the surrounding region, the ripeness of pomes, stone fruits and soft fruit is a decisive quality criterion for fine spirits. The best distillates can only be produced with a high-quality base product, such as fully ripe, healthy and clean fruit. After sorting and crushing the fruits, they are mashed, enzymes added, acidified and fermented with yeast. After alcoholic fermentation, the actual distillation process begins, during which the alcohol is removed from the mash by distillation and concentrated. This process is divided into the forerun, middle run and last run; the middle run is the actual distillate. An important factor during distillation is the time. Only with patience and experience is it possible to achieve the best results. The heating process is particularly slow to ensure that during the forerun, only the highly volatile and unwanted substances such as acetic acid esters and acetaldehyde are separated. If the master distiller heats too strongly during this process step, they will lose valuable flavors that absolutely must be preserved for the subsequent middle run. It is therefore important to heat at a constant rate. It is this part of the process which contains the value-adding and desired elements, such as aroma compounds and potable alcohol. The subsequent last run contains higher-boiling elements and is undesirable for the high quality of the end product and must be separated during distillation. During the filtration process which follows the subsequent distillate storage and adjustment to drinking strength, the Hiebl distillery relies on Eaton filtration solutions. “For this process, it is crucial to have a wide range of graded filter sheets available that we can select and combine,” explains Georg Hiebl. “We rely on the extensive range of filtration solutions from Eaton and we are also always very well advised and informed about the latest developments, which is of added value to our high standards.” 

Solution

Apart from a few exceptions when basically no filtration takes place, the majority of products are filtered. BECO SELECT A depth filter sheets and filters from the BECO standard range are used to remove the unwanted substances from the distillate. They are used for the sophisticated filtration of highquality spirits and offer distillers consistency in color, flavor and aroma. 

The BECO SELECT A depth filter sheets, with a nominal separation rate of 0.8 microns or 2.5 microns, are ideal for aroma-preserving filtration. This is achieved due to the high adsorption capacity for longand medium-chain fatty acid esters that cause hazing at higher filtration temperatures, the low adsorption of valueadding, short-chain fatty acid esters, and the high absorption capacity for fusel oils and essential oils. They also allow a secure separation of finelycolloidal to coarsely-dispersed solids and minimize crystalline precipitates such as calcium and magnesium hazing, metal hazing and carbon particles. The depth filter sheets thereby facilitate the pore structure and the use of high-quality raw materials. They are made from pure and natural materials with cationic charge carriers, such as finely fibrillated cellulose fibers from deciduous and coniferous woods, diatomaceous earth and perlits. They also have a low content of calcium, magnesium and iron ions in order to avoid secondary hazing and allow for a color-preserving filtration as there is minimal color adsorption in the depth filter sheet. This is an important aspect because the preservation of the natural color of cask-aged distillates, liqueurs or other colored spirits enhances their optical quality. 

The BECO standard depth filter sheets from Eaton provide a complete gradation in a retention range of 0.1 microns to 4.0 microns. These grades allow the filters to adapt very precisely to the respective individual requirements. They are used for coarse to fine filtration and thanks to their large-volume cavity structure, they have a high dirt-holding capacity and are therefore ideal for the filtration of coarse to very fine particles. 

At the Georg Hiebl distillery, this filtration is carried out in aroma-preserving temperatures between 4 and 8 °C, sometimes with very coarse filters. Two to five different filter strengths are used in each distillation and the filtrate is tested by means of blind tasting. It then becomes clear which filters and filter combinations are ideal for the particular requirements of each distillate. This is because the suitable filter strength depends on many individual factors such as the type and variety of fruit, the mechanical processing, the enzymatic digestion, the strength and duration of mixing, as well as the strength and method of distillation. So that the distillates remain stable when using coarser sheets, which only filter very slowly, a very gentle pump is used to carry out the filtration process at a correspondingly low pressure. 

The ultimate goal of the Hiebl brothers is to further improve the existing scent and flavor of the distillate, thereby achieving excellent results by means of a specifically attuned filtration. Aroma-concealing secondary tones, known as “veils”, and a bitter sensation which overwhelms the palate are reduced as flavor and odor are conserved, and mild to moderate bitter notes that enhance richness should be preserved. It is also important to maintain the sharp, fruity pressure on the palate, such as in the Williams Christ pear brandy. “With the BECO SELECT A depth filter sheets and the BECO standard range from Eaton, we have succeeded in exactly what we want to achieve in filtration: Getting the best results from fine distillates,” adds Georg Hiebl. 

Results 

These requirements are achieved thanks to Eaton filtration solutions and their selective use based on the extensive knowledge of the Hiebls. This successful combination has been recognized and honored hundreds of times over. The distillery has reached its initial goal, and will continue to pursue it – producing the finest distillates. In the process, it becomes particularly clear that, due to the time factor, which is also affected by the low rate of filtration, essential roles are played by temperature, selection and the combination of filter sheets. Thanks to the Hiebl brothers’ ability to specifically adapt these parameters, they create products with a great deal of flavor and aroma, a special sensory experience and high stability against cloudiness, resulting in distillates that are pure and clear with a track record for first-class “impeccable quality”.

BECO SELECT A depth filter sheets

They preserve premium ingredients in fine spirits and deliver consistent color, taste and aroma while virtually eliminating haze-causing substances.