下载文档 () / 20
动力,因我们而不同*

Location: Taiwan

Segment: Electronics Manufacturing 

Challenge: An ineffective air ventilating system was consuming huge amounts of water and did not improve air quality

Solution: An Eaton 32-inch Type 35L-CLC gas/ liquid separator capable of removing up to 99 percent of oil, water and other particles from a vapor

Results: A reduction in the oil mist/haze in the workshop, exhaust meets environmental standards, and a reduction in water related costs.

Background 

One of the world's largest manufacturers of touch panel screens, notebook covers and related electronics equipment reached out to Eaton to help it reduce environmental issues related to its sophisticated manufacturing process.

The Taiwan-based manufacturer believes that it has the most computer numerical control (CNC) machines in the world, and its international lineup of customers, which reads like a Who's Who in the computer and communications industries, helps support that claim.

Computer numerical control was introduced to the machining industry in the early 1970s. It has since revolutionized the way various metals are milled, lathed, drilled, cut and polished. The most basic function of any CNC machine is automatic, precise and consistent motion control.

Rather than applying completely mechanical devices to cause motion as is required on most conventional machine tools, CNC machines produce motion control via computer programming. All forms of CNC equipment have two or more directions of motion, called axes. These axes can be precisely and automatically positioned.

The CNC machining often uses lubricants to help diminish the high levels of heat typically generated in the process. Another downside is the vaporization of coolant, which often produces an airborne mist or haze. Though not believed to be a serious health hazard, the haze can make breathing uncomfortable and irritate eyes.

In addition, the mist cannot be released into the atmosphere according to local environmental protection laws. Doing so would result in substantial fines. Corporate sustainability mandates would also be compromised. 

Challenge

Eaton's customer was relying on an old and ineffective air ventilating system that consisted of a scrubber and plasma treatment equipment. Becoming increasingly more ineffective over the years, the two-step arrangement was also consuming huge amounts of water. That same water was being contaminated with oil residues and had to be transported to sewage treatment facilities. Meanwhile, the plant air quality did not improve.

Costly, dirty and encumbering quality, the system that kept tools and metals cool and lubricated needed to be replaced.

Eaton Filtration was recently summoned to clean up the mess. 

Solution 

An Eaton gas/liquid separator was installed to replace the outdated system to clear the air inside the manufacturing facility of that unpleasant mist. A 32-inch Type 35L-CLC was selected for the application, which is capable of removing up to 99 percent of oil, water and other particles more than four microns in size.

The self-contained two-stage design of the system functions by, first, increasing the size of liquid droplets through a wire mesh de-misting pad in the vessel's container. Next, the droplets are centrifugally thrown to the outside wall and flow to the bottom of the vessel for draining. The Eaton gas/liquid separator also prevents the droplets from being re-entrained after separation.

Additional features of the Eaton gas/liquid separator include:

  • High efficiency of oil mist removal.
  • No internal moving parts.
  • Reduced maintenance.
  • No media to be disposed.

Eaton boasts one of the world's largest inventories of filtration products. Designed for efficiency in a variety of demanding markets, applications, and environments, Eaton's lineup of filters includes pipeline basket strainers, mechanically cleaned filters and strainers, tubular backwashing filters, filter bags and bag filter housings, filter cartridges and cartridge filter housings, gas liquid separators, depth filtration, as well as hyd-raulic and lubrication oil filtration solutions to help optimize filtra-tion performance, quality and plant productivity. 

Results

After installation, oil mist/haze has been reduced to a minimum in the workshop, exhaust is meeting the necessary environmental standards, and the grease from the cooling liquids can be reclaimed and reused – an added benefit that was not possible with the old system.

Because no water is used with the Eaton separator, filtration costs have been reduced substantially, as have associated transport and disposal costs of contaminated water.

Employees at the site are also benefitting with cleaner, healthier working conditions, and Mother Nature is pleased by the absence of harmful emissions and water contaminates.

That's precisely what the company wanted.

Type CLC
Eaton’s 32-inch Type 35L-CLC gas/liquid separator 
The unique two-stage design removes 99% of all liquid and solid particles larger than 4 microns in size. Standard, one-stage separators are only capable of removing particles larger than 10 microns in size. The Eaton Coalescer Separator's efficiency far exceeds that of any other type of centrifugal, cyclone, turbine, or vane type separator.