How Supervisory Control and Data Acquisition (SCADA) revolutionizes electrical asset management
Supervisory Control and Data Acquisition, commonly known as SCADA, is an automated control system used in modern electrical systems to help drive more efficient operations. SCADA systems are designed to collect data from critical assets via sensors installed within equipment across an organization. Data can be processed and analyzed, and the output can be used to enable personnel to make, better, more informed decisions about the best course of action with their assets.
SCADA systems consist of software and hardware components that enable operators to gather data to efficiently monitor, control, and optimize electrical assets. These systems provide remote control for equipment monitoring processes, performance aberrations, and data analysis.
Communication networks are the backbone that connects components such as sensors, RTUs (Remote Terminal Units), PLC's (Programmable Logic Controllers), and the central controls in SCADA systems. These communication networks ensure data flows seamlessly between field devices and peripheral systems, enabling real-time monitoring and control.
Operational efficiency and electrical asset reliability are enhanced when a SCADA system is connected to equipment. The system can collect varying types of data from equipment, including temperature, pressure, or speed data. The data may then be analyzed and presented in a dashboard, and trends can be determined.
Such insights may then be used to take broader actions, allowing personnel to make better decisions.
A typical SCADA system will comprise several components, which include:
The electrical asset management space is taking a different shape with the advent of technological advancements such as the Internet, Internet of Things (IoT), Industrial Internet of Things (IIoT), Artificial Intelligence (AI), and big data analytics, all of which have influenced the versatility and improvement of SCADA systems.
To fully understand the evolution of a SCADA system, we must reflect on the days of manual monitoring and on-site staff presence to monitor asset conditions.
SCADA has evolved into Electrical Power Monitoring Systems (EPMS) due to the requirement for more detailed and specialized monitoring of electrical power systems. SCADA systems began to incorporate more advanced features specific to power monitoring, leading to the development of EPMS to address the growing demand for reliable and efficient energy management. Connecting SCADA and EPMS enables dependable operation of IT infrastructure by monitoring power distribution, spotting potential problems, and facilitating effective energy use in several verticals, such as data centers, where power management is essential.
SCADA and the Industrial Internet of Things (IIoT) are commonly contrasted, and some electrical asset analysts believe IIoT applications will eventually replace traditional SCADA systems. For classic SCADA systems, IIoT applications are generally regarded as alternatives, not replacements. IIoT applications can be installed on top of SCADA, decreasing the pitfalls of vendor lock-in, like a lack of standards and interoperability.
AI and machine learning algorithms can analyze large volumes of SCADA data to find trends and forecast future events. This information enables predictive maintenance for better asset condition decisions and enhanced overall efficiency of electrical systems. Integrating SCADA systems with IIoT devices makes a wider range of detailed data collection possible. This integration makes even more accurate electrical asset monitoring and control possible, making management techniques more relevant and adaptable.
AI and machine learning (ML) algorithms can analyze large volumes of SCADA data to find trends and forecast future events. This information provides predictive maintenance for better asset condition judgments and enhanced overall efficiency of electrical systems.
Incorporating advanced security features into future SCADA systems to guard against cyberattacks and guarantee the accuracy and dependability of electrical asset management is crucial.
As industries evolve to accommodate IIoT in electrical asset management, the need for automatic or proactive solutions continues to drive the development of the systems.
SCADA/EPMS has impacted the electrical asset management landscape in many ways, enabling multiple protocol connectivity, data analysis, real-time monitoring, predictive capabilities, and more.
The evolution of SCADA into EPMS represents a significant advancement in power monitoring and management. Electrical asset management tasks, such as machine monitoring, data collection, alert responses, and field device control, are carried out by conventional SCADA systems and Industrial Internet of Things (IIoT) applications in industrial settings.
However, there are distinctions between them, such as the lack of robust analytics capabilities that IIoT systems are known to exhibit.
The impact of SCADA/EPMS on electrical asset management is seen in several ways, which include:
All Eaton's Exertherm CTM solutions can be connected to SCADA/EPMS/BMS systems, enabling personnel interaction with data visualization and temperature trend analysis of monitored equipment.