下载文档 () / 20
动力,因我们而不同*

The role of CTM in asset integrity management (AIM)

What is asset integrity management (AIM)?

Asset integrity management, or AIM, is a holistic approach that ensures industrial assets' dependability, security, and efficiency throughout their operational lifecycle. The core objectives of AIM are to avoid equipment failures, adhere to regulations, and maximize the lifespan and effectiveness of critical assets across various industries.

Why is asset integrity management important?

Asset integrity management is important for many reasons, including minimizing risks and managing potential failures in electrical assets and other critical components in an organization's infrastructure. When these assets fail, it can lead to costly downtime, personnel safety hazards, and wider damage to the business.

Asset integrity management includes the following key components:

  1. Risk assessment: AIM performs rigorous risk assessments to detect potential faults that could be detrimental to the reliability of industrial assets. These include lifetime approaches for controlling the risk of corrosion, erosion, fatigue, and other issues.
  2. Maintenance strategies: This includes adopting practical maintenance approaches to maintain the excellent condition of assets. These practical maintenance approaches could include preventive maintenance, which is periodically done to address issues as they arise but before they escalate; reactive maintenance, when quick actions need to be taken; and predictive maintenance, using actionable data-driven insights.
  3. Inspection and monitoring: To ensure that asset integrity is maintained, applying inspection and monitoring approaches is crucial. This can include corrosion monitoring, non-destructive testing, and real-time sensor data for asset integrity monitoring measures.
  4. Personnel training: Providing relevant training guarantees the expertise of those working on asset management and integrity projects. Professionals with the appropriate skills and knowledge are essential for efficient asset management and risk reduction.
  5. Documentation and record keeping: This involves properly documenting records on the condition of assets by noting inspection results and maintenance activities. This is crucial because it provides trackable data on asset history, offering insights for future decisions and compliance standard maintenance.
  6. Regulatory compliance: In-service assets must typically follow industry and regulatory standards. These regulatory standards cover several areas of asset operation that include (but are not limited to) industry-specific requirements, asset integrity, and maintaining environmental and personnel safety in line with regulatory requirements.
  7. Continuous improvement: Facility owners are driven to ensure that outages due to mechanical failures or other equipment integrity factors are minimized because of how costly the negative impact can be. Ensuring that continuous improvement is maintained helps to monitor the integrity of assets with performance data and implement appropriate approaches to update maintenance procedures or make worn-out part replacements, guaranteeing the smooth running of assets.

The role of continuous thermal monitoring (CTM) in AIM

Continuous thermal monitoring (CTM) is revolutionizing asset integrity management (AIM). As an electrical asset maintenance approach, it facilitates the installation of thermal sensors in electrical assets to collect real-time data that helps operators predict potential faults before they occur.

CTM is an integral part of AIM, ensuring the dependability of assets for safety and optimal operation. CTM helps mitigate risks and reduce unnecessary maintenance, which helps reduce costs and optimizes overall operational efficiency.

The concept of continuous thermal monitoring includes the around-the-clock monitoring and analysis of temperature in and around critical assets, which helps in the early detection of anomalies, and provides insights that can help safeguard assets from unplanned equipment failures.

CTM is an integral part of AIM because of the following roles it plays in ensuring better asset integrity:

  • Early detection of anomalies and advance warning: Problems such as the overheating or thermal degradation that can result in asset failures are identified by CTM before issues occur. With an always-on approach to monitoring temperature changes, CTM sensors make it easier to identify an anomaly that may be a sign of a more serious issue. The prevention of more asset serious damage and the optimization of asset lifespan can depend on this early detection.
  • Preventive maintenance strategies: CTM forms part of an organization's preventative maintenance schedule,helping them move away from traditional asset maintenance approaches such as periodic inspections and manual assessments. When electrical assets exceed temperature limitations, it can lead to the degradation and structural failure of an asset. Organizations can then take steps to mitigate potential issues from the moment they are detected by continuous monitoring sensors, rather than run to failure or picked up during a planned maintenance interval. This strategy increases asset lifespan, reduces maintenance costs, and minimizes downtime.
  • Enhanced safety measures: In industrial processes, safety is of utmost importance. CTM plays a significant role in safety protocols by detecting temperature anomalies that could otherwise endanger personnel, assets, or the wider operational environment. Organizations can ensure a safer working environment by implementing better safety protocols through the implementation of sensors that will alert teams to compromised assets in advance of human interaction.
  • Data-driven decision making: Organizations can make well-informed decisions based on analysis and insights derived from real-time data that is provided by thermal sensors. The efficiency of asset management methods is increased by these data-driven insights, making it possible to prioritize maintenance tasks that reduce maintenance costs, improve resource allocation, and allow better decisions to be made.
  • Industry agnostic: CTM technology is applicable in various industries, including oil and gas, aviation, mining, chemical processing, and manufacturing. Its success as a universal industry solution for AIM is established by its adaptability to various applications and assets.
  • Integration with emerging technologies: CTM is a condition-based monitoring approach that has grown with technology development and keeps improving with the advent of the Internet of Things (IoT) and artificial intelligence (AI). CTM's capabilities are enhanced by incorporating automation, advanced analytics, and predictive insights, establishing its position as a cutting-edge AIM solution.

Continuous thermal monitoring (CTM) revolutionizes asset integrity management (AIM) by providing a proactive, data-driven, real-time strategy and actionable insights for protecting vital assets.

Organizations looking to maintain the integrity and durability of their industrial assets will find the Eaton Exertherm CTM solutions to be an invaluable solution due to the ability of our technology to continuously identify anomalies early on, improve safety protocols, maximize operational effectiveness, and have flexible adaptability to numerous industry types.

Continuous thermal monitoring will play an even more prominent role in determining how asset integrity management is practiced globally in the future as technology develops.

Would you like to know more?

Discuss your specific application requirements with our expert engineers, obtain additional technical information, or learn more about our other applications.

Related resources