下载文档 () / 20
动力,因我们而不同*
  • Continuous thermal monitoring for motor control centers

    Contact us

Transform MCCs into smart assets

Motor control centers (MCCs) are prone to failures from loose or compromised connections, often at the rear of the bucket or in-drawer joints, which are impossible to inspect without de-energizing. Traditional maintenance methods rarely catch these problems early. Many facilities only discover thermal faults when damage is severe and repairs become expensive. Continuous thermal monitoring (CTM) for motor control centers provides real-time visibility into MCC health, enabling proactive intervention before failures disrupt operations.

This solution is a fit if you need to:

  • Monitor hard to reach MCC power connections continuously
  • Reduce reliance on periodic inspection alone
  • Improve visibility into fault development between inspections
  • Add monitoring in retrofit or new-build MCC applications
cover-image-brochure-mcc-in-bucket.png

How the MCC monitoring solution detects thermal change

    1. The MCC datacard collects sensor temperature data to

      activate alarms when a fault is detected

    2. Non-powered sensors attach directly to the critical

      incoming / outgoing power connections where they

      continuously monitor temperature

    3. A simple LED display provides local and visual
      system status

    Inside MCC image

    Features of MCC ‘in-bucket’ monitoring solution

    The Eaton Exertherm continuous thermal monitoring for motor control center solution is the most advanced way to detect potentially compromised MCC assets before they fail and cause unexpected operational downtime, or worse, damage. Suitable for retrofit and new build installations, the in-bucket or in-drawer MCC solution provides protection from thermal asset changes where the eye can’t see and the hands can't reach. Our unique ‘fit and forget’ 24/7 electrical infrastructure monitoring technology gives you the peace of mind that your assets are running safely. 

    Benefits of MCC 'in-bucket' monitoring solution

    Continuous visibility at critical connection points

    Monitor hard-to-reach MCC power terminations in real time, where faults are most likely to develop but are difficult to detect.

    Simple deployment within MCC environments

    Designed for in-drawer and in-bucket installation, supporting both retrofit and new-build applications without complex modification.

    Reduced reliance on periodic inspections

    Move beyond snapshot-based maintenance with continuous monitoring that captures changes between inspection intervals.

    Improved personnel safety

    Minimize the need for manual inspection of energised MCC equipment, reducing exposure and supporting safer maintenance practices.

    eaton-thumbnail-optimizing-electrical-infrastructure-in-mining-brochure.png

    How continuous thermal monitoring (CTM) transformed reliability in a 24/7 mining operation

    See how it works: watch the MCC video

    MCC in-drawer / in-bucket solution

    1. MCC datacard

      Collects sensor data

    2. MCC status LED

      Displays current monitoring status

    3. MCC sensor loom

      Connects to key monitoring points within the MCC

    Eaton mcc kit numbering

    How alarms and monitoring data can be integrated into existing setup

    The MCC thermal monitoring ‘In-drawer’ solution can be connected in 3 ways.

    1. Relay only

      Local status LED visual with local/remote alarms

    2. Exertherm Thermal Xpert 25

      Local graphics on HMI and status LED with local/remote alarms, plus the transfer of raw data via Modbus TCP/IP

    3. Exertherm MCC aggregator

      Local status LED visual with local/remote alarms and the transfer of raw data via Modbus 485

    eaton-thumbnail-motor-control-centers-how-keep-oil-refineries-running-brochure.png

    Energy conglomerate replaced periodic thermography with always‑on proactive monitoring

    Why choose Eaton Exertherm for MCC thermal monitoring?

    Our CTM solution is designed as an OEM‑neutral solution to MCC thermal monitoring, enabling continuous visibility across motor control centre drawers and buckets regardless of manufacturer. It focuses on monitoring the hard‑to‑reach power connections where thermal faults are most likely to develop but are often difficult to detect using conventional methods.

    By providing real‑time insight into temperature change at these critical points, it helps teams identify developing issues earlier and improves visibility into fault progression between inspection intervals. Suitable for both retrofit and new‑build MCC environments, the solution integrates easily into existing electrical infrastructure and reduces the need for interaction with energized equipment during maintenance activities to support safer working practices.

    Need more info? Let's talk

    Get in touch to find out more about MCC thermal monitoring by filling in the form. One of the Exertherm team will reach out to learn more about your requirements as soon as we can.

    Frequently asked questions

    From the essentials to the more advanced, these are some of the questions we’re asked most often. Get in touch to learn more about MCC Monitoring Solution.

    Motor control centers (MCC) are known to be prone to failure caused by loose or compromised connections. The joints most susceptible to faults are typically at the rear of the MCC bucket/in-drawer, and impossible to access for inspection without de-energizing (especially in-drawers). Many facilities don’t realize they have thermal issues until it’s too late, and damage has already occurred, which can be inconvenient and costly.
    spacer
    Yes. Exertherm's MCC solution can be used for both new build motor control centers as well as retrofit existing assets. 
    spacer
    Annual thermography inspections are typically conducted annually, which is less than 1% of a monitoring cycle. This approach relies on luck to detect a failure during an inspection. It also exposes maintenance personnel to safety risks whilst inspecting. In addition to this, the detection of compromised joints is more challenging when assets are deenergized. The use of thermal imaging to detect temperature rise in a cooling joint can give unreliable results that are not indicative of the true state of a connection under load.
    spacer
    To achieve a true operational likeness, inspections need to be performed whilst equipment is energized rather than de-energized due to connections cooling down. As personnel carry out inspections, actively seeking out problematic electrical joints, they become exposed to the potential safety risks resulting from loose connections.
    spacer

    Our patented MCC solution monitors 24/7, 365 days a year, and delivers 100% ‘always on’ uptime visibility for critical connections. The solution enables early detection of overheating joints, which are an early indicator of electrical component degradation.

    The MCC solution is simple to install in new build or retrofit in existing equipment. The sensors operate as a standalone system, and use an algorithm to identify abnormal temperature rise before an electrical failure occurs. The solution also enables real time baseline data to be captured to provide trend analysis. 

    Permanently installed sensors remove the need for personnel to engage with energized equipment to carry out condition assessment, minimizing safety risks.

    spacer

    Traditional inspections typically require equipment shutdown to allow physical access, which can not only give unreliable results, but result in the inconvenience of downtime and lost productivity.

    Our ‘fit-and-forget’ thermal sensors offer a smarter alternative:

    • 24/7 real-time insights to help reduce unplanned downtime
    • Compliant by design with key safety standards such as NFPA 70B
    • No shutdowns - no recalibration - no ongoing maintenance

    Our solution supports predictive maintenance planning, keeping your operations safe, efficient, and audit ready.

    spacer
    Because it works, continuously. Continuous thermal monitoring (CTM) provides always-on, real-time insights that periodic inspections simply can’t match. That’s why every major OEM now recommends it as the standard for predictive maintenance helping facilities reduce risk, improve uptime, and stay compliant.
    spacer