下载文档 () / 20
动力,因我们而不同*

Supercapacitors versus batteries

 

Energy storage optimization in a connected world

The global connection of devices is a trend that spreads to “things”, allowing for the ability to remotely monitor and control equipment and devices. This trend has rapidly spread from industrial IoT (IIoT) systems supporting asset and process monitoring equipment to industrial automation, smart cities, smart homes, electric vehicles, and smart grids. In a nutshell, additional power, as well as power optimization, are more critical than ever in an increasingly connected world.

Supercapacitors vs. batteries

Conventional storage technologies such as lithium and alkaline battery technologies are becoming inefficient and unable to keep up with current and emerging technologies. For example, batteries are prone to overheating (resulting in thermal runaway), cranking issues (for vehicle engines in cold start conditions), and shorter lifetimes (both during storage and regular use). Due to their unique construction, Supercapacitors offer significant benefits over batteries including thermal stability, ultra-long life, and maintenance-free operation.

Supercapacitor modules come with pre-installed balancing circuits to ensure safe and optimal operation. Unlike battery management systems (BMS), these balancing schemes do not require external controls or monitoring. This allows for greater simplicity in integrating energy storage into applications, such as electric vehicles and smart grids, while also mitigating operational expenditures. 

How do supercapacitors work?

The working principle of supercapacitors is similar to that of standard capacitors. Basic capacitors store energy between two conducting plates or electrodes, separated by a non-conducting region or a dielectric. Supercapacitors store charges at the interface between an electrode and an electrolytic solution which creates a capacitor at each electrode. A supercapacitor essentially bridges the gap between a battery and a capacitor. Furthermore, supercapacitors exhibit much faster charging and discharging speeds than a battery while storing much more charge than an electrolytic capacitor.

 

The construction and applications of supercapacitors

This whitepaper discusses the construction of supercapacitors, their principles of operation, and various applications that they are ideal for.

Why choose supercapacitors over batteries?

There is a bevy of benefits to incorporating supercapacitors in electronic designs. These components can serve as sole energy storage or in combination with batteries to optimize the cost, efficiency, size, and longevity of diverse electronic products. Key benefits include smaller footprints, longer life, high energy density compared to an electrolytic capacitor, higher power capability than a battery, thermal stability, and a wide application range. 

Small energy storage footprint in next-generation IoT systems

The number of IoT end devices is projected to jump from the current 13.8 billion to nearly 31 billion -- a more than twofold increase by the mid 2020s. These massive machine type communications (mMTC) are defined by their low throughput and small payload wireless connectivity to enable high power, size, and cost-constrained sensor nodes. The high power capability of supercapacitors are ideal for IoT devices which require efficient energy storage but need pulses of energy for communications. Supercapacitors provide small form factor storage that last 2-4 times longer than batteries with high power density and no thermal runaway risk. 

Supercapacitors surpass batteries for power storage cycling

With current battery chemistries, lithium-ion and lead-acid types last only a few years and experience fast degradation due to chemical reactions and variances in operating and storage conditions. On the other hand, supercapacitors can achieve millions of charge/discharge cycles spanning up to two decades.

High energy density

High power density critical to meet the growing energy needs of modern applications. Like other passive components, supercapacitors often form the basic building blocks of electronic circuits. Key applications include pulse power, ridethrough power, graceful shutdown, hybrid energy storage systems (HESS) and backup power.

Improved thermal stability

Conventional batteries are notoriously susceptible to fluctuations in operating temperature. Batteries have been known to fail easily in cold or elevated temperatures, causing startup issues and costly downtime for time-sensitive operations. Failure and degradation due to battery chemistries and defects also result in thermal runaway. Supercapacitors ensure stable performance over a wide range of operating temperatures, enhancing the safety and reliability of electronic products.

Power applications of supercapacitors

Both small and large-sized electronic applications including IoT devices, data centers, industrial plants, healthcare facilities, and other public areas increasingly require the use of clean and quality power with little risk of downtime. In these applications, reliable sources of backup power even with short backup times in the event of power failures can avoid potentially catastrophic results of power variation, outage and downtime.

Energy storage and the environment

With growing and widespread concerns about the increasing deposits of toxic metals around the world and their effects on climate change, supercapacitors offer a robust, eco-friendly solution compared to traditional energy storage. Unlike batteries, supercapacitors provide clean energy storage without safety concerns, do not contain toxic metals or additional accessories or components, and are much simpler in terms of power management. 

Eaton supercapacitor resources

For more information on Eaton supercapacitors, please visit the available resources.

Want more information?

Fill out this form if you would like to be contacted by an Eaton Electronics representative.

提交本表格即表示,我同意我提供的个人数据可以根据伊顿隐私政策和适用的数据隐私法与伊顿、渠道合作伙伴和代表伊顿工作的第三方服务商共享。

I agree to be informed regularly about Eaton products, promotions and news. I understand and agree that Eaton will use my data to personalize marketing communications.  I agree that the personal data that I provide can be shared with Eaton Corporation plc in Ireland, Eaton Corporation in the United States of America and for storage in electronic marketing databases hosted in Canada. Any use of my personal data will take place in compliance with the relevant and applicable data privacy laws and the Eaton Privacy Policy. I can withdraw my consent to receive marketing communications at any time by contacting Eaton.