下载文档 () / 20
动力,因我们而不同*

Filtration of pharmaceutical ingredients

(Chemical synthesis)

Active Pharmaceutical Ingredients (APIs)

APIs (Active Pharmaceutical Ingredients) are combined or formulated with excipients to produce pharmaceutical or medical products. The production of APIs involves either biotechnological or chemical processes. In both cases, filtration plays a key role throughout the entire manufacturing process in ensuring the production of high-quality ingredients and pharmaceuticals.

Filtration of active pharmaceutical ingredients (APIs)

Learn more about Eaton´s solutions for the filtration of active pharmaceutical ingredients.
eaton-api-manufacturing-chemical-synthesis-graphic-en.jpg

1 - Separation

The chemical reactor is followed by the first separation phase. Solids, such as the catalyst bound to activated carbon, or other reaction byproducts are filtered out first. In addition to bag filtration, sheet or stacked disc cartridge filtration is particularly suitable. In many cases, the combination of BECO standard or BECOPAD depth filter sheets made of cellulose, in an enclosed frame filter, such as the BECO INTEGRA PLATE is the optimal solution for solids separation. If the requirements for chemical compatibility with regard to raw materials or sealing materials are higher, stacked disc cartridge filtration is recommended. A system consisting of BECODISC stacked disc cartridges and the enclosed BECO INTEGRA DISC stacked disc cartridge housing is a clean solution in this case. Optionally, the system can also be equipped with stacked disc cartridges with increased cell spacing.

2- Clarifying filtration

Following the solids separation, clarifying filtration takes place for the separation of fine particles. Depending on the desired purity of the filtrate, this step is carried out in several stages using a combination of stacked disc cartridge and cartridge filtration to protect downstream components.

3 - Crystallization

Active pharmaceutical ingredients are processed in the drug either in powder or in liquid form. There are therefore two alternative process routes.

In liquid form, the active pharmaceutical ingredients undergo various filtration steps after crystallization. BECOPAD depth filter sheets are ideal for the separation of fine particles and colloids, for the reduction and separation of microorganisms and for the protection of a final membrane filtration. The use of BECODISC BC activated carbon stacked disc cartridges with BECO CARBON depth filter sheets is recommended for the separation of undesirable organic by-products or decolorization.

Single-sheet filters such as the BECO INTEGRA SOLO are used in solids extraction after crystallization.

4 - Filling and Drying

A further, final filtration stage is carried out to protect the tank or container filling. Depending on the requirements, the liquid active ingredients are filtered using filter bags or filter cartridges.

Contact us

By filling out and submitting the form, I agree that the personal data that I provide can be shared with Eaton Corporation plc in Ireland, Eaton Corporation in the United States of America and with Eaton’s channel partners, and I agree to be contacted via phone or email by Eaton’s channel partners and/or a third party agency that Eaton works with in order to help route and answer the questions asked in the form. Any use of my personal data will take place in compliance with the relevant and applicable data privacy laws and the Eaton Privacy Policy.

提交本表格即表示,我同意我提供的个人数据可以根据伊顿隐私政策和适用的数据隐私法与伊顿、渠道合作伙伴和代表伊顿工作的第三方服务商共享。

Opt-in to marketing

I agree to be informed regularly about Eaton products, promotions and news. I understand and agree that Eaton will use my data to personalize marketing communications. Any use of my personal data will take place in compliance with the relevant and applicable data privacy laws and the Eaton Privacy Policy.  I can withdraw my consent to receive marketing communications at any time by contacting Eaton.