下载文档 () / 20
动力,因我们而不同*

Filtration pressure loss non-water calculator

Step 1 Enter your flow rate in GPM
Step 2 Enter C V value for your strainer size from C V Factors chart on the catalog page
Step 3 Select basket mesh size or select PERF for 1/32" to 1/2" perforation sizes  
Step 4 Enter the specific gravity of your liquid
(e.g. water=1.0)
Step 5 Select the viscosity of the fluid in SSU  
   
 
  Calculated pressure loss in PSI is:
  Calculations are done from reference data we believe to be correct, results should be verified for correctness.  

Additional tools