下载文档 () / 20
动力,因我们而不同*

Hybrid vehicle case study

The development and production of electric and hybrid vehicles has been on the rise over the last 2 decades and this trend is likely to increase exponentially over the next 20 years. As automotive manufacturers look to utilize cleaner, cheaper energy and meet CO2 regulations worldwide by 2020, electric and hybrid vehicles will become a much larger part of the market.

However, the power needed to run a vehicle combined with design needs for compact, lightweight inverters has made thermal management an important stumbling-block for automotive engineers and manufacturers. Thermal solutions for these power modules must be lightweight, small enough to fit within the power train, powerful enough to cool extremely hot components and cost efficient enough not to raise the price points on these vehicles.

To overcome these challenges, Infineon Technologies came to Eaton, for help in developing a cooling solution for their latest power module family, HybridPACK™ Double Sided Cooling (DSC) for hybrid and electric vehicles. Their dimensions and characteristics allow these modules to be more flexible with a compact design of the overall application and can dissipate heat on both sides of the module. Infineon and our European Design Center studied a concept for a liquid cooling solution able to provide the specific performance level.

The specifications for this application: power to be dissipated by each of the three DSC modules, electronic connections and integration, and boundary conditions. Starting from the characteristics of DSC modules and the requested thermal resistance and pressure drop, Eaton began the analysis of possible concepts of liquid cold plates (LCPs); the basic idea was to put one LCP on top and one LCP on the bottom, in order to cool the two active sides of each module.

Different key points have been considered: overall geometry, internal cooler structure, wall thicknesses, inlet and outlet position, top-bottom connection, mounting technique and target cost. The geometry has been defined by the main mechanical constraints: dimensions of the active area of DSC modules, available space around the modules and integration with the overall system.

The internal structure has been defined according to the requested performance level through thermal resistance and pressure drop. The key was to add an optimized flow turbulator in order to increase the exchange surface and the convection heat exchange coefficient, while keeping pressure drop under the established limit. The updated design was then simulated using computational fluid dynamics (CFD). The material thickness has been evaluated in order to withstand the requested operating and testing pressure. Further analysis was focused on the connection between top and bottom liquid cold plate and the position of inlet and outlet. At this stage, the connection between top and bottom has been considered external to the LCP itself, made by means of flexible tubes and clamps with each LCP with one inlet and one outlet port. This way the design can leverage a parallel connection between the top and bottom LCPs, with the advantage of having two equal parallel flows and consequently the same performance level on the two LCPs.

Finally, the mechanical clamping between top and bottom has been studied: considering the minimum clearance and creepage distances to be guaranteed, eight fixing points have been added, externally to the active exchange surface area. The mechanical connection between top and bottom can be done either with fast features such as rivets or with screws. Prototypes of this concept have been made in order to validate the thermal and mechanical analysis and the results of the experimental tests confirmed that it is suitable to withstand the requested pressure and to guarantee both the indicated thermal resistance and pressure drop. For the first prototypes, rivets have been used to clamp top and bottom liquid cold plates.

The concept developed by Eaton and the availability of prototypes enable the automotive industry to quickly design efficient inverters for hybrid and electric vehicles using Infineon HybridPACK DSC modules.

Project details

  1. Customer: Infineon
  2. Application: Electric and hybrid vehicles
  3. Technology: Liquid cooling
  4. Industry: Automotive
  5. Location: Germany