下载文档 () / 20
动力,因我们而不同*

Improving hyperscale UPS system reliability between inspection with continuous thermal monitoring (CTM)

Uninterruptible Power Supply (UPS) systems deployed in hyperscale environments are expected to operate continuously, at scale, and under variable load conditions, often across hundreds or thousands of distributed electrical assets. In these environments, UPS reliability is not a local concern; it is a systemic risk factor that directly impacts availability, safety, and operational continuity.

While inspections, performance monitoring, and redundancy remain essential, hyperscale operating models increasingly require continuous condition insight to manage risk that develops between verification events. One of the most significant and often underestimated risk to reliability in UPS infrastructure is thermal stress.

Why thermal stress in UPS is a primary reliability risk in hyperscale environments

In hyperscale environments, UPS systems operate under sustained load, frequent cycling, and evolving demand profiles. Over time, this creates thermal stress at electrical connection points such as joints, terminations, battery interconnects, and power electronics interfaces. These conditions rarely manifest as immediate faults; instead, they develop incrementally as resistance increases, and temperature rises under normal operation. Because hyperscale facilities prioritise uptime and limit intrusive access, these early‑stage conditions often remain undetected.

At scale, this creates compound risk:

  • Small thermal issues increase the likelihood of fleet-wide UPS risk
  • Degradation occurring silently between inspection cycles
  • Escalation detected late, when intervention options are limited
Inadequate monitoring and management of overheating can result in catastrophic failures, shorten battery life, and damage internal components.

Why periodic inspection does not mean protected for UPS infrastructure

Periodic inspection programs remain essential for UPS maintenance, compliance, and safety. However, inspections are inherently point-in-time activities. They capture asset conditions under a specific load profile on a specific day and do not reflect how electrical connections behave as operating conditions evolve. In live UPS environments, access constraints and extended inspection intervals create an unavoidable inspection blind spot.

This is a period after an inspection and before the next one where emerging electrical risk continues to develop unseen.In modern UPS environments operating continuously under variable load, relying solely on periodic inspection assumes risk develops slowly enough to be captured at the next scheduled check. When faults emerge between inspections, visibility arrives late and response becomes reactive, increasing operational risk despite compliance with inspection schedules.

Challenges of periodic electrical inspection 1

Preventing thermal risks in UPS with continuous thermal monitoring

Continuous thermal monitoring (CTM) provides around-the-clock visibility into temperature behavior at critical electrical points within UPS systems. Rather than relying on periodic inspections or point-in-time thermography, continuous monitoring observes how temperature evolves under real operating conditions, enabling the detection of abnormal thermal trends before escalation occurs. This enables operators to detect abnormal thermal trends, not just absolute thresholds.

In practice, this allows hyperscale operations teams to:

  • Identify overheating components before failure risk escalates
  • Perform targeted validation instead of broad inspections
  • Prioritise intervention based on trend severity and real-time data on asset health, not assumptions

This proactive approach reduces the likelihood of unplanned UPS failures, power events, and safety incidents without increasing operational disruption.

Extending UPS battery life in large-scale deployments

Battery performance is particularly sensitive to temperature, making thermal visibility essential in large UPS utilized facilities. Sustained exposure to temperatures outside recommended operating ranges rapidly increases chemical degradation, reducing service life and increasing replacement frequency across fleets.

For example, lead‑acid batteries still widely used in many UPS architectures operate optimally between 68°F and 77°F (20°C to 25°C). Sustained exposure above this range accelerates chemical degradation, shortening battery lifespan and increasing replacement frequency.

At hyperscale, even marginal temperature deviations can:

  • Significantly reduce battery service life across fleets
  • Increase maintenance cycles and material costs
  • Introduce variability into reliability planning

Continuous thermal monitoring (CTM) enables early identification of localized hotspots and environmental deviations, supporting more consistent battery performance and predictable lifecycle management across large deployments.

How UPS systems and thermal monitoring work together in data centers

Power management in modern mission-critical environments like data centers is increasingly complex. Facilities may contain thousands of servers, drawing high electrical loads and generating substantial heat. UPS systems must operate continuously under fluctuating demand while maintaining stable power delivery.

While installing a UPS system provides a foundational layer of protection, permanently installed thermal monitoring sensors help ensure the long-term reliability and smooth operation of critical electrical assets.

Some advanced monitoring tools also provide thermal trend data and heat‑mapping capabilities, helping teams prioritize attention and avoid damage before it occurs.

As UPS estates scale, manual inspection regimes become increasingly resource intensive. Thermal monitoring supports a shift toward condition-based maintenance by reducing reliance on calendar-driven inspections and enabling remote oversight of UPS thermal health. Frequent physical inspections are not always feasible in live environments and often provide limited incremental insight.

For hyperscale operators, this improves efficiency while maintaining strict reliability standards.

Thermal monitoring complements UPS infrastructure by:

  • Observing how components behave under real operating conditions
  • Identifying thermal hotspots that inspections may miss
  • Supporting proactive, predictive maintenance strategies

Thermal monitoring supports a shift toward condition‑based maintenance by:

  • Reducing reliance on calendar‑driven inspections
  • Enabling remote oversight of UPS thermal health
  • Highlighting where attention is genuinely necessary

A practical guide to continuous, 24/7 risk monitoring in data center power systems

Eaton Exertherm CTM solutions for hyperscale UPS environments

Heat remains one of the greatest threats to the lifespan and reliability of UPS systems, particularly in high‑load, always‑on critical infrastructure environments such as data centers.

Eaton Exertherm continuous thermal monitoring solutions are designed to address this risk by providing always‑on temperature monitoring of critical UPS components.

Exertherm CTM solutions:

  • Continuously track temperature at vulnerable electrical points
  • Detect abnormal thermal behavior early
  • Support condition‑based maintenance strategies
  • Reduce unplanned downtime and unnecessary maintenance activity

By identifying temperature anomalies before escalation, CTM helps operations teams maintain UPS reliability, improve safety, and protect critical operations.

Designed for live operational constraints

In hyperscale data center environments and other always-on critical environment, retrofit feasibility determines whether a solution is usable.

Eaton Exertherm continuous thermal monitoring solutions are designed to be:

  • Retrofit‑compatible across existing UPS systems
  • Deployable incrementally, not all at once or on day one
  • Aligned with site procedures and maintenance windows

In most cases, installation is carried out during planned maintenance periods, with only the affected UPS modules or sections safely isolated rather than impacting the entire site. Deployment can be prioritized to address the highest-risk locations first, with coverage expanding over time as part of a broader reliability programme.

This allows for improved visibility without large-scale disruption. It also enables seamless integration into existing maintenance strategies, while reducing operational risk during deployment.

Related resources