下载文档 () / 20
动力,因我们而不同*

Continuous thermal monitoring (CTM) for oil and gas electrical systems

Oil and gas facilities depend on electrical reliability to sustain production, processing, compression, transport, storage, and marine operations. When an electrical asset fails, the impact is rarely isolated. A fault in switchgear, a motor control center, transformer, UPS, or power distribution asset can affect output, maintenance response, safety planning, and operational continuity across wider parts of the facility.

Continuous thermal monitoring (CTM) addresses this risk by monitoring temperature behavior continuously at critical electrical connection points. Instead of waiting for the next inspection, engineers can see abnormal temperature rise as it develops and prioritize intervention before a fault becomes an outage, equipment failure, or unsafe maintenance event.

Why CTM matters in oil and gas

Oil and gas operations concentrate many of the conditions that make electrical risk difficult to manage. Upstream assets may operate offshore, in remote fields, or in harsh environments where access is limited and inspection windows are constrained.

Midstream infrastructure relies on electrical systems to support compression, pumping, transport, and distribution. Downstream facilities such as refineries, petrochemical plants, and LNG terminals depend on stable power to maintain tightly controlled process environments.

In each setting, electrical faults often begin quietly. A loose connection, overloaded circuit, deteriorating termination, or heat-stressed component can continue operating while risk increases in the background. By the time a problem becomes visible through an outage, alarm, smell, visible damage, or manual inspection, the condition may already have progressed into a more disruptive and costly event.

This is why real-time thermal visibility of electrical assets matters. CTM helps teams move from inspection-led awareness to continuous condition awareness. It does not remove the need for maintenance discipline, but it gives decision-makers better information between inspection intervals and under real operating load.

Eaton thumbnail motor control centers how keep oil refineries running brochure

Energy conglomerate replaced

periodic thermography with

always‑on proactive monitoring

Inspection alone is no longer enough

Inspection-led maintenance provides important evidence, but it leaves long periods of time unmonitored. In oil and gas facilities, this gap matters because electrical behavior changes with load, environment, operation, and asset condition. A component that appears acceptable during inspection may begin deteriorating before the next scheduled check.

Continuous monitoring does not make inspection irrelevant. Instead, it makes inspection more informed. CTM helps teams understand where risk is developing so physical inspection, investigation, or intervention can be focused where it is most needed. This reduces waste, improves prioritization, and supports a more resilient maintenance strategy.

How CTM supports predictive maintenance

Many oil and gas organizations are moving away from purely time-based maintenance because fixed intervals can result in over-servicing some assets while hidden degradation continues elsewhere. CTM supports a more predictive and condition-based approach by providing continuous temperature data that reflects how assets behave in real operating conditions.

When thermal trends are visible, maintenance teams can identify early signs of deterioration, review whether conditions are worsening, and plan intervention before failure occurs. This shifts the maintenance conversation from “when is the next inspection due?” to “which asset is showing evidence of developing risk?”

For reliability teams, this means better use of maintenance labor, stronger prioritization of critical assets, and clearer justification for corrective action. For operations teams, it means fewer surprises and better alignment between maintenance activity and production priorities.

AttributePeriodic thermography

Continuous thermal monitoring

Asset visibilityProvides a snapshot of asset condition at the time of inspection.Delivers continuous visibility into electrical asset behavior between inspections and under real operating conditions.
Fault developmentThermal issues may remain undetected until the next inspection cycle.Identifies abnormal temperature rise as it develops, enabling earlier intervention before production is affected.
Maintenance planningMaintenance decisions are based on inspection findings and fixed schedules.Supports condition-based maintenance using real-time asset health and trend data.
Safety exposureIncreases interaction with electrical assets during inspection activities.Reduces unnecessary exposure to energized equipment by providing visibility between inspection intervals.
Decision basisRelies on inspection reports and periodic condition assessments.Uses live temperature data and thermal trends to support more informed maintenance decisions.

What engineers and operations teams gain in day-to-day practice

The bigger strategic benefit of CTM is that it helps oil and gas organizations move from reactive or inspection-led maintenance toward a more resilient condition-based approach. Eaton presents continuous thermal monitoring not as a replacement for all maintenance activity, but to supplement and strengthen existing practices with always-on thermal insight. The goal is to make maintenance more informed, timely, and safer.

For electrical engineers

CTM adds a layer of asset intelligence that is difficult to achieve with periodic inspection alone. It helps reveal where thermal stress is forming, supports troubleshooting with live condition data, and creates historical temperature trends that can be reviewed over time. This makes it easier to distinguish one-off anomalies from recurring deterioration and to decide where intervention is justified based on actual risk.

For operations teams

The value is equally clear. Stable power availability is essential to production continuity, and operations teams need to know that risk is being tracked between maintenance intervals. Continuous monitoring supports earlier fault detection, faster identification of developing issues, and more informed prioritization of corrective actions. Instead of spreading inspection effort across both healthy and compromised assets, teams can focus resources where thermal behavior shows risk is increasing.

Many oil and gas organizations are moving away from purely time-based maintenance because it can lead to over-servicing some assets while hidden degradation continues elsewhere.

Continuous thermal data gives teams the basis for condition-based maintenance. Trends can be reviewed, warning thresholds can be managed, and maintenance can be aligned with asset condition rather than fixed intervals alone.

Where will you use CTM?

CTM delivers the greatest value in oil and gas environments where electrical continuity is critical and where hidden thermal faults can have disproportionate consequences.

Related resources